Release Name: MCUXpresso Software Development Kit (SDK)
Release Version: 2.2.2
Package License: LA_OPT_NXP_Software_License.htm - Production Use, Section 2.3 applies

CMSIS Core header files    Author: ARM                                       
                           parentversion: 4.5                                
                           URL: http://silver.arm.com                        
                           name: CMSIS Core header files                     
                           Format: source code                               
                           License: Open Source - BSD-3-Clause               
                           Location: CMSIS/Include                           
                           version: 4.3 (CMSIS Download 4.5)                 
                           Description: Industry-standard header files       
                           distributes by ARM for cortex-M cores             

DMA Manager                Format: source code                               
                           Location: middleware/dma_manager_2.1.0            
                           Description: A software component used for manage 
                           on-chip DMA channel resources.                    
                           name: DMA Manager                                 
                           License: Open Source - BSD-3-Clause               
                           version: 2.1.0                                    
                           Author: Freescale                                 

FatFs                      Approved Open Source License: Yes                 
                           Author: Electronic Lives Mfg. by ChaN of Ageo     
                           city, Japan (hobbyist)                            
                           Description: FatFs is a generic FAT file system   
                           module for small embedded systems.                
                           Format: source code                               
                           License: Open Source - FatFs License,             
                           <rootfolder>/middleware/fatfs/doc/en/appnote.html 
                           Location: middleware/fatfs_0.12c                  
                           name: FatFs                                       
                           URL: http://elm-chan.org/fsw/ff/00index_e.html    
                           version: 0.12c                                    

FreeRTOS(tm)               Author: Real Time Engineers, Ltd.                 
                           Description: A real-time operating system(RTOS)   
                           from Real Time Engineers, Ltd.                    
                           Format: source code                               
                           License: Modified GPLv2. See                      
                           ,<rootfolder>/rtos/freertos/License/license.txt.  
                           Location: rtos/freertos_9.0.0                     
                           name: FreeRTOS(tm)                                
                           URL: http://www.freertos.org                      
                           version: 9.0.0                                    

HostSDK                    version: 1.8.1                                    
                           Location: tools/wireless/host_sdk                 
                           Description: Network Protocol stack serial bus    
                           drivers and application code                      
                           License: Open Source - BSD-3-Clause               
                           URL: https://opensource.org/licenses/BSD-3-Clause 
                           Origin: NXP                                       
                           name: Connectivity Host SDK                       
                           Format: Binaries, source code and header files    

KSDK CMSIS Peripheral      Author: Freescale                                 
Drivers                    version: 2.x.x                                    
                           Format: source code                               
                           Description: CMSIS Peripheral drivers are designed
                           to provide hardware independent APIs which make   
                           application reusable across a wide range of       
                           supported microcontroller devices.                
                           name: KSDK CMSIS Peripheral Drivers               
                           Location: devices/<device>/cmsis_drivers          
                           License: Open Source - Apache 2.0 & BSD-3-Clause  

KSDK Peripheral Driver     Description: Peripheral drivers are designed for  
                           the most common use cases indentified for         
                           the underlying hardware block.                    
                           Author: Freescale                                 
                           Version: 2.x.x                                    
                           License: Open Source - BSD-3-Clause               
                           Format: source code                               
                           Location: devices/<device_name>/drivers           

Kinetis_BLE                version: 1.3.6                                    
                           Location: middleware/wireless/bluetooth_1.3.6     
                           Description: Bluetooth Low Energy Software        
                           License: Open Source - BSD-3-Clause               
                           URL: https://opensource.org/licenses/BSD-3-Clause 
                           Origin: NXP                                       
                           name: Bluetooth Low Energy Application Source     
                           Format: Source code and header Files              

Kinetis_BLE_ControllerLib  version: 4.2.6                                    
                           Location:                                         
                           middleware/wireless/bluetooth_1.3.6/controller/lib
                           Description: Bluetooth Low Energy Controller      
                           Firmware. Host Command Interface (HCI).           
                           License: Proprietary, LA_OPT_NXP_Software_License 
                           - Production Use, Section 2.3 applies             
                           Origin: Mindtree                                  
                           name: Bluetooth Low Energy Controller Firmware    
                           Format: Binary libraries                          

Kinetis_BLE_HostLib        version: 1.3.6                                    
                           Location:                                         
                           middleware/wireless/bluetooth_1.3.6/host/lib      
                           Description: Bluetooth Low Energy Stack (HCI,     
                           L2CAP, ATT, GATT, GAP and SM)                     
                           License: Proprietary, LA_OPT_NXP_Software_License 
                           - Production Use, Section 2.3 applies             
                           Origin: NXP                                       
                           name: Bluetooth Low Energy Host Firmware          
                           Format: Binary libraries                          

Kinetis_Demo_Apps          version: 1.3.6                                    
                           Location: tools/wireless/binaries                 
                           Description: Kinetis Wireless Demo Applications   
                           License: Proprietary, LA_OPT_NXP_Software_License 
                           - Production Use, Section 2.3 applies             
                           Origin: NXP                                       
                           name: Kinetis Wireless Demo Applications          
                           Format: Binaries                                  

Kinetis_FWK                version: 5.4.6                                    
                           Location: middleware/wireless/framework_5.4.6     
                           Description: Kinetis Connectivity Framework       
                           middleware for Connectivity stacks                
                           License: Open Source - BSD-3-Clause               
                           URL: https://opensource.org/licenses/BSD-3-Clause 
                           Origin: NXP                                       
                           name: Kinetis Connectivity Framework              
                           Format: Source code                               

Kinetis_FecLib             version: 5.4.6                                    
                           Location: middleware/wireless/framework_5.4.6/DSP/
                           FEC/lib_fec_IAR_*.a                               
                           Description: Connectivity FEC Library for Kinetis 
                           License: Proprietary. LA_OPT_NXP_Software_License 
                           - Production Use, Section 2.3 applies             
                           Origin: NXP                                       
                           name: Connectivity FEC library                    
                           Format: Binary libraries                          

Kinetis_GENFSK             version: 1.1.6                                    
                           Location: middleware/wireless/genfsk_1.1.6        
                           Description: Software for driving the GENFSK      
                           Module                                            
                           License: Open Source - BSD-3-Clause               
                           URL: https://opensource.org/licenses/BSD-3-Clause 
                           Origin: NXP                                       
                           name: Generic FSK Link Layer Software             
                           Format: Source code and header files              

Kinetis_SecLib             version: 5.4.6                                    
                           Location: middleware/wireless/framework_5.4.6/SecL
                           ib/lib_crypto_*.a                                 
                           Description: Connectivity Security Library for    
                           Kinetis                                           
                           License: Proprietary, LA_OPT_NXP_Software_License 
                           - Production Use, Section 2.3 applies             
                           Origin: NXP                                       
                           name: Kinetis Connectivity SecLib                 
                           Format: Binary libraries                          

Percepio Tracealyzer -     version: 3.0.9                                    
Snapshot Demo              Location: boards/<board>/rtos_examples/visualizati
                           on/freertos_percepio_snapshot                     
                           Description: Percepio Tracealyzer                 
                           License: Open Source - BSD-3-Clause               
                           Author: Percepio                                  
                           name: Percepio Tracealyzer - Snapshot Demo        
                           Format: source code                               

SD MMC Card middleware     name: SD MMC Card middleware                      
                           Location: middleware/sdmmc_2.1.2                  
                           License: Open Source - BSD-3-Clause               
                           Description: A software component support SD card,
                           eMMC card.                                        
                           Author: Freescale                                 
                           version: 2.1.2                                    
                           Format: source code                               

Segger SystemView Demo     version: 2.40a                                    
                           Location: boards/<board>/rtos_examples/visualizati
                           on/freertos_segger_sysview                        
                           Description: Segger systemview demo               
                           License: Open Source - BSD-3-Clause               
                           Author: Segger                                    
                           name: Segger SystemView Demo                      
                           Format: source code